AXIS#.IL.FRICTION

Description

Position command derivative sign is multiplied by this value to be injected to the current command.


  • AXIS#.IL.FRICTION is active in Position and Velocity modes (OPMODE = 1, 2), but not active in Torque mode (OPMODE = 0).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0 to the minimum of user positive current limit (AXIS#.IL.LIMITP) and motor peak current (AXIS#.MOTOR.IPEAK ).

Default Value

0

Data Type

Float

See Also

AXIS#.IL.FF

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.FRICTION

500ah

0bh

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5808

1

5808 (0x16b0)

AXIS1.IL.FRICTION

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.FRICTION

5808

Float

Read/Write

-